Software download for tools
   



Evaluation Software


Upgrades


Utilities


  Sample Codes  


 
HEW (High-performance Embedded Workshop) V.3.01.06

Supported Products

This version supports the following products.

  • SuperH RISC engine C/C++Compiler packages
    • R0C40700XSW09R
    • R0C40700XSW08R
    • P0700CAS7-MWR
  • H8S, H8/300 series C/C++Compiler packages
    • R0C40008XSW06R
    • PS008CAS5-MWR
  • C compiler packages for the M32R MCU family
    • M3T-CC32R V.4.20 Release 1 through V.4.30 Release 00
  • C compiler package for the M32C/80, and M16C/80 MCU series
    • M3T-NC308WA V.5.20 Release 1
  • C compiler packages for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, and R8C/Tiny MCU series
    • M3T-NC30WA V.5.20 Release 1 and V.5.30 Release 1
  • C compiler packages for the R8C/Tiny MCU series (freeware Products)
    • M3T-NC30WA V.5.20 Release 1 (*)
    • M3T-NC8C V.5.30 Release 1
      NOTE:
      * This product's name was changed from M3T-NC30WA to M3T-NC8C on April 1, 2004.
  • E10A-USB emulators
    • HS0005KCU01H
    • HS0005KCU02H
  • E7 emulator
    • HS0007TCU01H
  • E6000H emulator
    • HS7058EPH60H and others
  • E6000 emulator
    • HS3664EPI62H and others
  • E10A emulator
    • HS7705KCM02H
    • HS7729RKCM02H
    • HS7750RKCM01H
    • HS2378KCM01H and others
  • E10T emulator
    • HS3048BTCM01H
    • HS3048BTCI01H and others
  • E200F emulator
    • R0E0200F0EMU00

Updater Function

1.Functions Improved

(1) For the Set Monitor command (monitor_set, a command for setting and displaying monitoring points)

(a) The function of displaying the syntax on the command line has been improved. (This function instructs you how to set parameters of each command on-screen.)

(b) Changes have been made to the displays of the states of monitoring points.

  • Displaying the setting order of command parameters omitted.
  • The options of the Initial_value command parameter have been changed from TRUE/FALSE to enable/disable. (Initial_value determines whether to display the contents of memory or not as a default at opening the Monitor window.)

(2) The error message that appears if the connection with the target is canceled by the user or cannot be established has been changed from "Target Missing" to "Target Missing or Connection Canceled."

2. A Problem Encountered at Installing Products with Which a HEW Is Included Resolved

The following problem arising at updating products with which a HEW is include has been resolved: Products cannot properly be updated in some PCs with either of the following error messages beingdisplayed:

  • An error has arisen during the execution of the setup program.
  • Insert Floppy Disk 1 containing the layout.bin file.

For details, visit the Web page at

http://tool-support.renesas.com/eng/toolnews/hew/notes.html

3. Other Problems Fixed

The following problems have been fixed:

(1) If the last label in ASCII order is searched for using the search function (*) in the Label window, the error message "LABEL NOT FOUND" appears.

* This function becomes available by following these steps:

  1. Right-click an unoccupied area in the Label window
  2. A pop-up menu appears.
  3. Select the Search command in this menu.

(2) If multiple-step execution is discontinued and then the program is executed in the usual way, the STOP button on the toolbar for manually stopping the program stays not illuminated, which may disable the manual stopping of the program.

At the same time, such operations of the HEW may not be managed as closing the workspace by selecting the File → Close Workspace command or ending the application by selecting the File → Exit command.

For details, see RENESAS TOOL NEWS "A Note on Using Integrated Development Environment HEW--On Discontinuing Multiple-Step Execution" issued on August 16, 2004 at

http://tool-support.renesas.com/eng/toolnews/n040816/tn2.htm

(3) The status of the Connect up to target on debug go check box (*) cannot be kept when the session is saved.

* To see this check box, open the Options menu and select the

Debug Settings command. The Debug Settings dialog box appears, and then select the Options tab in it.

(4) Using the Open Workspace command in the interface of the HEW's server function (*) may cause an application error to arise.

* For details of the HEW's server function, see HewServer Document.

(5) If load modules written in the ELF/DWARF2 format are downloaded and the source file containing them is displayed in the Source window, the addresses of the source lines in which no program statements are written may incorrectly be provided.

For details, see RENESAS TOOL NEWS "A Note on Using Integrated Development Environment HEW--On Debugging Load Modules Written in ELF/DWARF2 Format" issued on August 16, 2004 at

http://tool-support.renesas.com/eng/toolnews/n040816/tn1.htm

(6) The Set History function of the Monitor Setting dialog box (*) in the Monitor window is unavailable.

* To see this dialog box, open the View menu and select the CPU, Monitor, Monitor Setting command. Or, right-click an unoccupied area in the Monitor window. A pop-up menu appears, and then select the Monitor Setting command in it.

(7) When two or more Monitor windows (those displaying the contents of memory in real time) are opened, debug sessions are saved, and then the saved sessions are reloaded, the Monitor windows opened at the second and later display the incorrect contents of memory.

For details, see RENESAS TOOL NEWS "A Note on Using Integrated Development Environment HEW--On Saving Debug Sessions in Monitor Windows" issued on September 1, 2004 at

http://tool-support.renesas.com/eng/toolnews/n040901/tn3.htm

(8) When files written in assembler language are opened in the HEW's Editor window, syntax coloring may not function properly.

For details, see RENESAS TOOL NEWS "A Note on Using Integrated Development Environment HEW--On Syntax Coloring of Specified Character Strings" issued on July 16, 2004 at

http://tool-support.renesas.com/eng/toolnews/n040716/tn3.htm

(9) The name of the M3T-PD30SIM simulator debugger does not appear in the External Debugger list box in the NewProject-5/6-Setting the Target System for Debugging dialog box.

For details, see RENESAS TOOL NEWS "A Note on Using Integrated

Development Environment HEW--On Selecting an External Debugger at Creating Projects" issued on July 16, 2004 at

http://tool-support.renesas.com/eng/toolnews/n040716/tn6.htm

(10) Context-sensitive helps (*) may be unavailable when the following tabs are selected in their respective dialog boxes:

  • The Build and Editor tabs in the Options dialog box
  • The Toolbars, Placeholders, Debugger, Log, and Help tabs in the Customize dialog box
  • The Options tab in the Debug Settings dialog box

* Click the "?" mark at the top right of each dialog box, and then click any item in it (for example, the Edit box). You see a help relevant to the item pops up.

Download

Please save "hewv3161u.exe" in an appropriate folder and execute it.

(53,152KB)

Notes
  • When more recent HEW than HEW V.2.2 is not installed, it is not updated to the HEW V.3.01.06.
  • Any components (Tool chain, Simulator, etc.) other than the HEW are not updated.
  • In use of SuperH RISC engine C/C++compiler package (P0700CAS7-MWR), please update to the HEW V.3.01.06 after upgrading a compiler package to V.7.1.03 or V.7.1.04.
  • In use of H8S, H8/300 series C/C++compiler package (PS008CAS5-MWR), please update to the HEW V.3.01.06 after upgrading a compiler package to V.5.0.05 or V.5.0.06

Uninstallation

In the list of the [Add/Remove Programs applet] in the [Control Panel],compilers and emultors are registered as "Hi-performance Embedded Workshop". (This name may be slightly modified by the types/versions of the products) This program is registered as "High-performance Embedded Workshop Updater",different from the above programs.

Uninstallation method

1. Uninstall "High-performance Embedded Workshop Updater"

2. Uninstall "High-performance Embedded Workshop3." If the files and start menus weren't deleted, delete it manually with using explorer.

 

© 2005 Renesas Technology Corp., All Rights Reserved.