HEW (High-performance Embedded Workshop) V.3.01.05
Supported Products
This version supports the following products.
- SuperH RISC engine C/C++Compiler packages
- R0C40700XSW08R
-
P0700CAS7-MWR
- H8S, H8/300 series C/C++Compiler packages
- R0C40008XSW06R
- PS008CAS5-MWR
- C Compiler Package for the M32R Family MCUs
- M3T-CC32R V.4.20 Release 1 and V.4.20 Release 1A
- C Compiler Package for the M32C/80 and M16C/80 Series MCUs
- M3T-NC308WA V.5.20 Release 1
- C Compiler Package for the M16C/60, M16C/30, M16C/Tiny, M16C/20,
M16C/10,
and R8C/Tiny Series MCUs
- M3T-NC30WA V.5.20 Release 1 and V.5.30 Release 1
- C Compiler Package for R8C/Tiny Series MCUs only (Freeware)
- M3T-NC30WA V.5.20 Release 1 (*)
- M3T-NC8C V.5.30 Release 1
NOTE:
* This product's name was changed from M3T-NC30WA
to M3T-NC8C on April 1, 2004.
- M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, R8C/Tiny series
- M3T-NC30WA Professional version
- M3T-NC30WA Free version
- E10A-USB emulators
- HS0005KCU01H
- HS0005KCU02H
- E7 emulator
- E6000H emulator
- E6000 emulator
- E10A emulator
- HS7705KCM02H
- HS7729RKCM02H
- HS7750RKCM01H
- HS2378KCM01H and others
- E10T emulator
- HS3048BTCM01H
- HS3048BTCI01H
- E200F emulator
Updater Function
1. Function of Generating Make Files Improved
In relation to the dependencies of include files on a source file, directory
information on include files has hitherto been output to a Make file
using relative path names if the nesting levels of include files are
less than 11. In this revision, this limitation is raised to less than
51 in the nesting levels. (If they are equal to or greater than 51, absolute
path names used.)
2. A Problem Encountered at Installing Products with Which a HEW is included
Resolved
The following known problem has been resolved: No project types for builds
cannot be displayed in the Project Type list box of the New Project
Workspace dialog box if, after installing any compiler package including
a HEW, the E7 emulator software product is installed without invoking the
HEW at all.
For details, go to A
Problem Still Remaining in the HEW 3.
3. Other Problem Fixed
The following known problems have been fixed:
- If comments in Japanese are included in a source line, a jump made from
the Navigation window to the line in the Editor window that declares
or defines a source file may reach an incorrect line locating several lines
after the destination.
- If a project that contains source files written in assembly language is
opened with the navigation function being activated, the automatic
analyses of the navigation function will not terminate.
For details, see RENESAS TOOL NEWS "A Note
on Using Integrated Development Environment HEW--On the Navigation Function" issued
on July 16, 2004.
- In the E10A, E10A-USB, or E200F emulator, if the OK button is pressed in
the Trace Branches dialog box (*) in the Trace window with the Enable option
button for source complement clicked, an application error arises while the
Progress dialog box is opening.
NOTE:
*This dialog box can be opened when you right-click any area of
the Trace window to display a pop-up menu and select
the Trace Branches command on the menu.
- In the E10A, E10A-USB, or E200F emulator, if the OK button is pressed in
the Trace Branches dialog box with the Enable option button for source complement
clicked; then an item of trace information is double-clicked to make a
jump to a source line in the Trace window, an application error arises.
- In the E200F emulator, if you select "BUS/MFI trace" from the
Trace Window list box in the Select Trace Window dialog box, an application
error arises.
Note that if you select "BUS/MFI trace" after once selecting "Internal/AUD/User
memory trace" from the Trace Window list box, no application error
arises.
- In the E200F emulator, if the OK button is pressed in the Trace Branches
dialog box in the Trace window with the Enable option button for source complement
clicked, the Progress dialog box is opened; then the contents of the Source
column is displayed in the Timestamp difference column while the complemented
trace information is being displayed.
Download
Please save "hewv3151u.exe" in an appropriate
folder and execute it.
(51.111KB)
Notes
- When more recent HEW than HEW V.2.2 is not installed, it is not
updated to the HEW V.3.01.05.
- Any components (Tool chain, Simulator, etc.) other than the HEW are not updated.
- In use of SuperH RISC engine C/C++compiler package (P0700CAS7-MWR),
please update to the HEW V.3.01.05 after upgrading a compiler package to V.7.1.03
or V.7.1.04.
- In use of H8S, H8/300 series C/C++compiler package (PS008CAS5-MWR), please update to the HEW V.3.01.05 after upgrading a compiler package to V.5.0.05
or V.5.0.06
Uninstallation
In the list of the [Add/Remove Programs applet] in the [Control Panel],compilers and emultors are registered as
"Hi-performance Embedded Workshop". (This name may be slightly modified by the types/versions of the products)
This program is registered as "High-performance Embedded Workshop Updater",different from the above programs.
Uninstallation method
1. Uninstall "High-performance Embedded Workshop Updater"
2. Uninstall "High-performance Embedded Workshop"
3. If the files and start menus weren't deleted, delete it manually with using explorer.