HEW (High-performance Embedded Workshop) Ver.3.0.02
The High-performance Embedded Workshop (HEW) was updated
to Ver.3.0.02 on December 15, 2003. Descriptions and how to update
are shown below.
Supported Products
This version supports the following products.
- SuperH RISC engine C/C++Compiler
packages
- R0C40700XSW08R
- P0700CAS7-MWR
- M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10, R8C/Tiny series
- M3T-NC30WA
Professional version
- M3T-NC30WA
Free version
- H8S, H8/300 series C/C++Compiler
packages
- R0C40008XSW06R
- PS008CAS5-MWR
- E10A-USB emulators
- HS0005KCU01H
- HS0005KCU02H
- E7 emulator
Descriptions
- Enhancement
- Navigation function
Category "C++ Classes" of the navigation function is
unchecked as a default.
- Problem Fixed
- Problem fixed at HEW termination
We have fixed the problem that the HEW did not quit normally.
Read This Before Downloading Update Program
The installer of the update program (hewv3002u.exe)
released on November 20 had the following restrictions.
Therefore, we have fixed the problems and updated the program (hewv3002u2.exe)
for the HEW Ver.3.0.02 on December 15. Because we revised the installer
only and the HEW is not modified, the version number is the same as
the previous one.
And, if you have successfully installed the update program (hewv3002u.exe)
released on November 20,
you do not need download the new update program (hewv3002u2.exe)
released on December 15.
Restrictions of the Update
Program (hewv3002u.exe)
for the HEW Ver.3.0.02 Released on November 20.
- In the following cases, you cannot update the HEW Ver.3.0.02.
- Updated from Ver.1.0.00 to Ver.2.0.02
- Updated from Ver.1.0.00 to Ver.2.0.02 (via Ver.2.0.01)
- With the following products, you cannot update the HEW Ver.3.0.02.
- Professional
version and Free version
of C compiler M3T-NC30WA for the M16C/60, M16C/30, M16C/Tiny,
M16C/20, M16C/10, R8C/Tiny Series
Ver.3.0.02 Download
How to Update
HEW Ver.3.0/Ver.3.01 -> HEW Ver.3.0.02
(11,097KB)
Notes
- When the HEW Ver.3.0 or HEW Ver.3.01 are not installed, it is
not updated to the HEW Ver.3.0.02.
- Any components (Tool chain, Simulator, etc.) other than the
HEW are not updated.
- In use of SuperH RISC engine C/C++compiler package (P0700CAS7-MWR),
please update to the HEW Ver.3.0.02 after upgrading a compiler
package to Ver.7.1.03 or Ver.7.1.04.
In use of H8S, H8/300 series C/C++compiler package (PS008CAS5-MWR),
please update to the HEW Ver.3.0.02 after upgrading a compiler
package to Ver.5.0.05 or Ver.5.0.06.