|
|
 |
|
 |
|
|
 |
 |
 |
| |
 |
Masaki Yamakawa
Group Manger
Image Processing Group
Image Engine Technology Department
Advanced Technology Research Laboratory
Mitsubishi Electric Corporation |
The image quality of LCD TVs continues to improve despite falling prices and broader product ranges. One reason for this is the rapid progress being made in the signal processing technology incorporated into LSI devices like the "digital video processor-multi" (DVP-M) series of video signal processing ICs jointly developed by Mitsubishi Electric and Renesas. These LSIs are the first to successfully combine all of the main signal processing functions for an LCD TV in a single chip. Their enhanced capabilities eliminate or greatly reduce the problems of blurred color and after-images previously associated with LCD screens. |
| |
| One chip integrates the functions of up to six ICs |
| |
| Flat-screen LCD TVs are an area of high consumer interest and the focus of intense competition among electronics manufacturers. Product lines are expanding and prices are falling, even as the picture quality and performance of these TV sets is improving. A tremendous amount of research and development effort is being expended to find ways to deliver more viewer satisfaction for less money. And that R&D effort is paying important dividends.
For example, five signal-processing functions are required for the LCD TVs currently being developed at Mitsubishi Electric Corporation. Technologies for Y/C separation, noise reduction, and IP conversion are essential. Additionally, compression feed-forward driving (cFFD) techniques improve video responsiveness, while natural Color Matrix (NCM) technology provides natural color reproduction with vivid colors. The new TVs also incorporate other functions, two are which being developed by Renesas: support for text broadcasting systems from different countries and an LCD-panel timing controller (TCON).
Previously, it took from two to six separate LSI devices to implement these seven functions. To simplify TV designs and cut costs, Mitsubishi Electric and Renesas have collaborated to develop the "digital video processor-multi" (DVP-M) series of video signal processing ICs. These complex devices are the first in the world to provide all of the previously mentioned technologies in single-chip solutions that deliver outstanding functionality and enhanced capabilities.
The DVP-M series LSIs eliminate or greatly reduce the problems of blurred color and after-images previously associated with LCD screens. Additionally, they save circuit-board space, cut power consumption, reduce parts counts and decrease overall cost. Figure 1 compares the old design with the new one. |
| |
| Applying the latest image processing technology |
| |
| Technology for achieving high image quality is a key to gaining a competitive edge in TV manufacture. Mitsubishi Electric has acquired strong expertise in image reproduction and has applied its extensive LCD TV know-how throughout the DVP-M series.
One example relates to the depiction of diagonal lines, which has been a weak point for LCD TVs. Contour correction technology that analyzes the characteristics of diagonal lines is used to improve the sharpness of contours. Generally, the signal processing of diagonal lines has consisted only of comparing vertically adjacent pixels and checking along the time axis. The new video signal-processing ICs do more. To improve the image, they apply technology that reduces edge widths by checking edge regions three-dimensionally, including diagonally adjacent pixels. The right-hand side of photograph 2 shows the resulting gain in image quality.
Another example of Mitsubishi Electric’s expertise is the use of cFFD technology to improve responsiveness and deal with the problem of after-images caused by the display screen's slow response speed. According to Masaki Yamakawa of Mitsubishi Electric's Advanced Technology Research Laboratory, "The cFFD technology optimizes the voltage applied to the LCD to boost response speed by comparing the 'before' and 'after' images when a change in image content means that a quick response is required. The result is a response speed of 12 to 14ms, which improves after-image performance to a realistic level. The cFFD technology also uses image compression techniques to reduce the required memory size to a level that makes it possible to integrate the circuitry on a single chip.".
Another feature of DVP-M series is that the devices provide video interfaces for three different broadcast standards: NTSC, PAL, and SECAM. This simplifies the process of developing LCD TVs for different regions of the world. |
| |
| Three device types — all single-chip implementations |
| |
To enable a wide range of end uses, from standard to high-end TV models, the LSI product range is split into three separate types of signal processing devices:
DVP-M devices are high-end chips that support W-XGA panels. They deliver maximum image quality because they use 3D processing for the Y/C separation, employ cFFD technology and have noise-reduction and IP-conversion functions. The DVP-M devices have 64Mbit of DRAM and are built with the proven Renesas solution integration product (SIP) technology shown in photograph 1.
DVP-MT versions support XGA panels, so they have fewer features and only 16Mbit of DRAM. They’re also built with Renesas SIP technology.
DVP-ML versions offer the most basic set of features.
All devices in this product line have the same pinouts for complete mechanical compatibility. Mr. Yamakawa comments that "because the chips are pin-compatible, a common platform (circuit board) can accommodate all three models in the DVP-M series. This reduces the cost and shortens the time required to develop a wide range of LCD TVs, from standard models to premium products."
The Renesas SIP technology that makes the pin compatibility possible has the added benefit of reducing the amount of wiring on the circuit board. In turn, this reduces issues related to electro-magnetic interference (EMI), easing system design.
|
| |
| Successful product launch spurs additional development |
| |
| The DVP-M series has enjoyed an encouraging start, having already been selected for use by a number of customers. A new DVP-MW device that supports dual display screens is currently under development. Additional research and development is progressing on an LSI for the large, high-quality LCD TVs that will become customers' flagship models.
Having established a successful collaboration, Renesas and Mitsubishi Electric will continue to work to facilitate the evolution of LCD TVs. Both firms are contributing their expertise for tuning the parameters of advanced DVP-M chip implementations.
|
| |

Photograph 1: In the DVP-M series LSI device, 64MB of DRAM is layered using Renesas SIP technology. |
|
| |

Photograph 2: There is a substantial improvement between the image on the left, produced by the previous vertical interpolation processing technique, and the one on the right, produced with the contour correction technology provided by the DVP-M series signal processor. IP conversion processing technology with diagonal line recognition smoothes diagonal lines. |
|
| |

Figure 1: The diagram on the left shows the complex circuit used by previous LCD signal processing techniques. The simplified, performance enhanced implementation with a DVP-M device is on the right. |
|
| |
|
|
|
© Copyright 2005, Renesas Technology, All Rights Reserved. |
 |
|