EDGE
 
2005.1/vol.8
BACK NUMBER
Special
System Solution
R & D
FOCUS ON
Products Information
Views on
International Network
PDF DOWNLOAD
 
 
 
- 64-MHz M32C/95 Group Microcontrollers
- SH7619 Processor with MAC and Ethernet PHY transceiver
- Two-chip Power MOSFET Device
- New Users: LG Electronics Applies SH-Mobile Application Processor
 
64MHz M32C/95 Group Microcontrollers for Automotive and Industrial Applications Launch Top-end M32C/90 Series in M16C Family
 
Left picture: 144-pin LQFP
Right picture: 100-pin LQFP
Offering twice the speed of chips in the M32C/80 group, these 32-bit devices have up to 768KB of flash, a three-channel CAN interface and many other peripherals

The M32C/90 series, the top of the range in the M16C family, comprise 32-bit CISC microcontrollers for automotive and industrial applications. The first product release consists of four 64MHz models in the M32C/95 group, which deliver twice the speed and more functionality than chips in the current M32C/80 series.

The new devices maintain the key advantages of the M16C family: highly efficient C language support, strong noise immunity, low noise emissions, and low power consumption. To improve processing performance, their high-performance M32C/90 CPU core has new features, including a 32-bit arithmetic circuit, transfer instructions, and a barrel shifter for shift instructions.

The microcontrollers provide a three-channel CAN controller. One channel of this controller supports 32 message slots, while the other two support 16 message slots. An on-chip non-stop debugging interface connects to an external debugger via a single unused pin. The devices' many other peripheral functions include 16-bit timers, DMAC, and A/D and D/A converters. Seven serial I/O channels provide LIN master support for systems equipped with communication functions. The two flash memory options are available: 768KB and 512KB. Development support includes the single-line non-stop debugger. The devices have 100-pin LQFP or 144-pin LQFP packages.

Click here for more details

 
Microprocessor with Internal Ethernet LAN Connection Function Simplifies Audio-Visual, Office Automation and Factory Automation Equipment
 
The SH7619, first single-chip device to include a MAC and PHY transceiver, is ideal for systems that offer 10/100Mbps Ethernet LAN connectivity

The SH7619, which expands the SuperH family, is a 32-bit microprocessor with an internal Ethernet PHY (physical layer) transceiver and Ethernet controller. It is an excellent choice for digital AV products, OA machines, and FA equipment that require a network connection function.

The new chip is the first Renesas microprocessor to incorporate both a media access controller (MAC) that complies with the IEEE-802.3 standard and a PHY transceiver on a single chip. (Previously the PHY was a separate component.) Thus, the SH7619 simplifies the development of 10/100Mbps Ethernet LAN connection functions and reduces the system component count. The chip's SH-2 CPU core has a maximum operating frequency of 125MHz and is suitable for the high-speed processing of TCP/IP and other protocols.

The microprocessor also includes a host interface function (HIF) for connecting to other microprocessors. An on-chip debug function supports real-time debugging at the chip’s maximum operating frequency. Development tools include the E10A-USB emulator. The SH7619 is packaged in a small (13mm x 13mm) 176-pin BGA.

Click here for more details

 
Power MOSFET Device Reduces Number of Components Needed in High-current DC/DC Converters
 
Left picture: Top
Right picture: Bottom
The HAT2210WP combines two MOSFETs in a low-thermal-resistance, WPAK-profile package; it can control 1.5x the output current of the HAT2210R device

The HAT2210WP power MOSFET enables the design of smaller DC/DC converters for notebook PCs, communication equipment, and many other types of products. The device contains two MOSFETs in a 5.3mm x 6.1mm package with a slim (0.8mm, max.) WPAK housing (Renesas profile code) that achieves high heat dissipation.

Heat generated by the power MOSFETS is transferred very efficiently to the circuit board from the heat-dissipating die pad on the under side of the device. In fact, the thermal resistance of the WPAK profile package is half that of the SOP-8 profile package used by the previous HAT2210R MOSFET device. As a result, the new HAT2210WP device can safely control one and a half times as much output current. System engineers can take advantage of this performance to reduce the number of MOSFETs in DC/DC converters that handle higher currents.

Also, because the HAT2210WP includes separate high-side and low-side transistors, it has separate drain connections. Both of the power MOSFETs are eighth-generation designs built with Renesas' latest industry-leading 0.35?m process. The optimized design of this power device emphasizes switching speed for the high-side transistor and low on-resistance for the low-side transistor. This makes it possible to obtain higher efficiency for the low-voltage side of the DC/DC converter.

Click here for more details

 
New Users: SH-Mobile Application Processor Is Used in Handset and Latest FOMA Models from LG Electronics
 
Besides being adopted for successive LG Electronics' mobile phones for international markets, the processor has been chosen for three manufacturers' 901i Series-3 handsets for the Japanese market

The SH-Mobile application processor has been selected for use in a GSM/EDGE handset produced by LG Electronics Corporation now on sale in the United States. (EDGE = Enhanced Data Rates for GSM Evolution, an enhanced data transfer technology based on GSM). Thus, there are now six different mobile phone models made by LG Electronics that use SH-Mobile devices, including a CDMA handset and a GSM/GPRS handset released since July 2004.

In the Japanese market, Renesas SH-Mobile chips have also been selected for the SH901iC (made by Sharp Corporation), the F901iC (made by Fujitsu Corporation), and the D901i (made by Mitsubishi Electric Corporation) ? three 901i Series-3 handsets for the NTT DoCoMo third-generation FOMA mobile phone service. These new handsets have been released progressively since December 2004. They provide long battery life: up to 570 hours of continuous standby operation (static) and 160 minutes of continuous communication time. Other features include a 260,000-color QVGA main color display, a 204Megapixel (max.) auto-focus digital camera function, and a seamless TV telephone function.

Click here for more detail

 
top
Global Site North America Europe Japan Singapore/ASEAN Hong Kong China Taiwan Korea Other Asian
© Copyright 2005, Renesas Technology, All Rights Reserved.