| 2-4 System Registers |
  |
This section describes the system registers.
Program Counter (PC)
This is the counter for instruction pre-fetch.
Procedure Register (PR)
This register stores the return address from a subroutine procedure. It
stores the return address in the procedure register when a subroutine is
called. Therefore in SuperH there is no memory access in a subroutine call
and no instruction pipeline stall. If it is nested 2 or more levels it is
the programmer's responsibility to save and restore the procedure register.
Multiply and Accumulate (MAC)
These registers store the results of multiply operations and multiply-and-accumulate
operations. If the result is to be used for other than a multiply and accumulate
operation it must be transferred to a general register. |
|